Hi all,
I have the following questions.
Please, Let me know the questions .
1) I got 4096 data from my " SD3GDAIII kit.".
I read 4096 times to read in 4096 16 bits values and store these values like this(0, 6063,6144........ )
I calculated…
Other Parts Discussed in Thread: LMH0394 , LMH0366 The LMH0394 and LMH0366 can both be operated in SPI mode and they can also be 'daisy-chained' as outlined in their respective datasheets. Is it possible to daisy chain an LMH0394 then LMH0366, then LMH0394…
Part Number: LMH0376 Other Parts Discussed in Thread: LMH0346 , LMH0366 , , LMH1226 , LMH0318 , LMH0397 , LMH1219EVM Hello TI support,
I'm looking for a 3G-SDI reclocker (to reclock 3G-SDI inputs coming into our board) that have, the following features…
Greetings,
1). Could you please specify what standard is it that requires 130nS of jitter? LMH0366 is an SDI reclocker and as far as i know SDI requires much less jitter.
2). You can DC and AC couple between the equalizer and the reclocker(LMh0366…
Hi Madhu,
The positioning of the LMH0346 looks appropriate.
Typically, the reclocker is placed in one of two locations, and it looks like your implementation uses Choice (1):
1. After the Cable EQ device and before the FPGA or Cable Driver
2…
Hi Jay,
LMH0303 and DS30BA101 are pin compatible. The main difference is that LMH0303 drives 75 ohm coax while DS30BA101 drives 100 Ohm differential line.
Please note LMH0366 is very sensitive to PCB layout especially when you have multiple LMH0366…
Other Parts Discussed in Thread: LMH0394 , LMH0366 , LMH0346 What is the proper method of attaching a balun or transformer to the front end of the lower power LMH0394 (2.5V) or similar. Input for this part is showing (typically) that it is capacitive…
LNIC
The LMH0341 is a deserializer which only deserializes data at 270Mbps, 1.5Gbps or 3 Gbps. It will not operate with MADI. If you need a reclocker that will operate at MADI rates, please look into the LMH0366 which is a dedicated reclocker, which…
Alpha, the LMH0394 requires an external termination resistor (and AC coupling capacitor) on the input, but nothing on the output.
The LMH0366 does not require termination resistors on the inputs or the outputs.
The LMH0302 will require a 100 Ohm termination…
Other Parts Discussed in Thread: LMH0394 , LMH0303 , LMH0366 , LMH0341 , DS32EL0124 Hello: Can I use the nominally SDI parts such as LMH03xx for an arbitrary protocol at 3 Gbps? Are these parts somehow dependent on the specifics of the video SDI protocol…