Part Number: LMH1208 Tool/software: Dear Team,
I am using the LMH1208 as a single cable driver, utilizing only the SDI_OUT1± output.
In this configuration, the SDI_OUT2± and OUT0± outputs are not used.
Could you please confirm whether it is acceptable…
Part Number: LMH1208 Other Parts Discussed in Thread: LMH1297 , LMH1226 , LMH1219 , LMH1218 , LMH1228 , LMH1297EVM , LMH1229 Tool/software: We are being asked to design a 3U 160 mm card with e 75-ohm BNC to 100-differential convertor. The signal speed…
Part Number: LMH1219 Other Parts Discussed in Thread: LMH1208 , Hello,
I have an application that need to use EQ for HD-SDI from 1 signal to 4 signals and I need an advice which option is better.
for what I can see there is 2 options which the LMH1219…
Part Number: LMH1208 I have seen many applications of the SDI interface and I understand the termination schemes of transmitting over a single coax and terminating the other output capacitively into 75 ohm. The same is then done at the receiver.
However…
Part Number: LMH1208
Hello,
Customer wants to use RS-170(NTSC/PAL) input and make 4 outputs as below diagram.
Is it possible to make this configuration?
If above configuration is available,
1. Can select LMH1208 output as 12G, 3G, HD or SD…
Greetings,
I am assuming this is 12G SDI signal? Do you have a scope shot of the LMH1208 75-ohm output?
Please note LMH1208 SLEW_CTRL should match data rate. Is this taken care of ?
I also noticed you are using closely coupled differential traces…
Part Number: LMH1297 Other Parts Discussed in Thread: LMH1219 , LMH1208 , , LMH1228 , LMH1218 Hello,
Our customer is looking for LMH1208 and LMH1219 single chip solution product. Then he has a question if LMH1297 can work as 12G UHD-SDI driver and 12G…
Part Number: LMH1208 Other Parts Discussed in Thread: LMH1228 , LMH1297 , LMH1219 Hi Team,
LMH1208 will be used for long distance transmission with cables, could you please tell the driving ability? How long the cable could be driven?
Thanks and Best…