Part Number: LMH6639 Other Parts Discussed in Thread: TLV8541 Tool/software: Please tell me about the LMH6639.
When I supply a 3.3V power source to the op-amp and the SD pin input is 0V, there is a momentary output from the op-amp.
After that, the output…
Other Parts Discussed in Thread: LMH6639 , LMH6642 Hello,
According to the data sheet of LMH6639 it has "Excellent Overdrive Recovery". I didn't find any information in the data sheet about recovery time from overdrive.
Can you help me with…
Other Parts Discussed in Thread: LMV116 , TLV9151 , LMH6639 , LMV7219 , TLV3201 , TLV3501 , TMUX1219 Hi team,
I need to convert a 1Mhz square wave VIN whose VH is 0V and VL is -0.2V to a 1Mhz square wave as VOUT1 or VOUT2 which is shown below. The phrase has…
Part Number: LMH6611 Other Parts Discussed in Thread: LMH6639 Hi Team,
I would like to know the Absolute Maximum Ratings "VIN Differential" specified value of LMH6611/2.
For example, I found that the LMH6639 data sheet has Absolute Maximum…
Dear Hasan
LMH6639 will not meet our bandwidth and slew rate requirment.
1. If we will generate 5V0 from 12V0 then are there parts which can fulfill our requirement i.e. meeting bandwidth requirement along with current requirement.
2. I have found One…
Hi Daniel,
Thanks for the reply. The ALM2402Q1 or ALM2402F-Q1 looks interesting and should be fast enough. I also found the LMH6639 which is an excellent match in typical specification but not guaranteed maximum. I think we'll give one or both of these…