Hey Karem,
1. Not sure why you are trying to apply the LMH6881, wouldn't a DAC be what you really want? That is what the THS3217 is intended to be used with
2. If you have a blocking cap at the LMH6881 inputs, you are not DC coupled and cannot get…
Part Number: LMH6517 Other Parts Discussed in Thread: LMH6521 , LMH6881 , LMH6515
Hi,
I'm looking for a VGA solution to satisfy the requirements below:
1. support 5V supply
2. gain step size:0.5-1dB
3. gain range: -10dB to 15dB
4.BW: DC-130MHz…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: LMH6881 , , SN74LVC1G14 , SN74LVC2G14 , SN74LVC3G14
Hi team,
Need to level shift a 0V logic 0 reference to -1.25V logic 0 reference for the LMH6881 device SPI working with max 50MHz SCLK frequency…
Hi Emmanouil,
Sorry for the delay in reply.
You should be able to DC-couple the LMH6881 output directly into the ADS4225 input by level shifting the LMH6881 supplies.
For 0.95V ADC input CM, the LMH6881 supply can be set to +3.5V/-1.5V in-order…
Part Number: LMH6518 Other Parts Discussed in Thread: LMH6881 Hi
Currently using VGA as LMH6518 (below is the circuit for the same). The output of this is given as the input for the ADC LTC2191.
As per datasheet the maximum output swing at the VGA…