Part Number: LMK61E0M Other Parts Discussed in Thread: LMK00334 Hi!
I'm using the LMK61E0M in my design. I'm attempting to do a signal analysis on this part of my circuit.
I'm looking for the IBIS file for this part so I can do the simulation.…
Part Number: LMK61E0M Other Parts Discussed in Thread: CDCE913-Q1 Hi,
I am looking for a programmable clock range from 25 MHz to 50 MHz frequency for Q grade with or without spread spectrum. Any suggestion? Or do you have any LMK61E0M for Q grade?
Aa…
Part Number: LMK61E0M Hello Clock Support Team,
When I using the LMK61E0M, how do I handle the unused OUT1? I want to use only OUT0. In this case, is it okay to just open the OUT1?
Best regards,
Alice
Matthew,
Can you provide an idea of the frequencies that you need to generate? A part such as the CDCM6208 (4 integer divider outputs, 4 fractional divider outputs) may be suitable here.
For a programmable oscillator, the LMK61E2 is suitable for LVPECL…
Part Number: LMK61E0M Hi,
Datasheet shows that Output frequency at LVCOMS 3.3V is from 50MHz(min) to 200MHz(max). My cusotmer wants to use LMK61E0M with 12.5MHz or 24MHz or 25MHz or 48MHz. Can LMK61E0M use under those condition?
What does below spec mean…
Hi Thanh,
Correct, LMK61E0M or LMK6C would be the best device we have for an LVCMOS oscillator. LMK6C is a fixed-frequency part so it would be easier and cheaper to design in. LMK61E0M requires programming so it's a little more complicated but it would…
Part Number: LMK61E0M Other Parts Discussed in Thread: USB2ANY Hi,
My customer is considering using LMK61E0M. And customer wants to change frequency on customer board by using GUI for EVM.
I think this is possible by the following constitution. Is it…
Hi Kailyn,
Correct, TICSPro only has a profile for the LMK61E0M. R21 can be manually changed according to the LMK61E2 register map to select the desired output type. The rest of the registers should me shared between LMK61E0M and LMK61E2.
I will review…
Hi Ying,
The 941AS EVM uses LMK61E0M , which operates up to 200MHz.
For Automotive grade, depending on your application configuration, you could also look into the following parts: CDCE913-Q1 , CDCEL937-Q1 , CDCE6214-Q1
Regards,
Fadi A.
Hi Deryck,
The factory programming of the LMK61E2 should output 156.25 MHz LVPECL by default. Can you provide a schematic of the circuit?
The recommended sequence to program the device is to write all the registers, issuing a stop command to skip all…