Hi Zhonghui,
The only LVCMOS oscillator we have available currently is LMK61E0M - https://www.ti.com/product/LMK61E0M
Unfortunately this doesn't support 500 MHz. That is a quite a high frequency for LVCMOS, generally speaking we've only seen CMOS type…
Part Number: LMK61E2EVM Other Parts Discussed in Thread: LMK61E0M , LMK61E2 , CODELOADER Hello,
where I can find the profile for LMK61E2EVM in TICS PRO?
Under: Select Device -> Oscillators
I only found LMK61E0M
Version of TICS Pro is v1.7.2.0
Many…
Part Number: LMK61E08 Other Parts Discussed in Thread: LMK61E0M , LMK61E2 , CODELOADER , LMK61E2EVM Hello everyone,
The datasheet in the chapter 9.2.2.3 Device Programming says:
"The EVM softwaretool TICS Pro/Oscillator Programming Tool can be used to program…
Part Number: DS90UH941AS-Q1 Other Parts Discussed in Thread: LMK61E0M Hi Team,
We used internal CLK to achieve internal Patgen. (following the https://www.ti.com/lit/an/snla132g/snla132g.pdf?ts=1624449102212&ref_url=https%253A%252F%252Fwww.google.com%…
Hi Elisha,
Checked with my colleague, we suggest use TICS Pro as we don't support CodeLoader anymore.
In the menu bar of TICS Pro --> Select Device --> Oscillators --> LMK61E0M.
LMK61E0M and LMK61E2 is almost 100% software compatible.
HI Andrew,
The LMK61E0M GUI in TICS Pro can be used to generate the commands. Attached is the configuration as a TICS Pro file and hex registers file. LMK61E0M 100M.tcs
LMK61E0M 100M.txt
R0 0x0010
R1 0x010B
R2 0x0200
R8 0x08B0
R9 0x0901
…
Hello Alexandre,
During the device qualification, we used LMK61E0M as the REFCLK source for external REFCLK mode which allows for programming a precise and flexible frequency based on system tuning (that is also included as an optional stuffing component…
Hi Shlomi,
If the output clock needs to synchronize with the 10MHz input clock, then CDCE913 is the simplest solution.
Otherwise, you can simply use an oscillator such as LMK61E0M.
Other Parts Discussed in Thread: LMK61E2 , LMK61E0M Can I generate a 41.68Mhz from programmable oscillator?
1. Need sine wave of this freq.
2. Can programmable oscillator drive a power amplifier. Can share the datasheet if required.
3. Can it be programmed…