Part Number: LMKDB1120 We are designing in the LMKDB1120Z100 for a 100 ohm differential clock distribution application and need phase noise data to complete our jitter budget.
The datasheet (SNAS855F) provides additive RMS jitter numbers and PSNR spur…
Part Number: LMKDB1120 Tool/software: Hi E2E,
Could you kindly help to check the question from customer as below? I also loop customer in.
What is the function of this pin? And what situation we need to enable it.
BR,
Janet
Part Number: LMKDB1120 Other Parts Discussed in Thread: CDC3RL02 Hi team,
Does LMKDB1120 include LDO like BAW oscillator does? If so, my customer can reduce the filter for power supply of LMKDB1120.
Best regards,
Shunsuke Yamamoto
Part Number: LMKDB1120 Tool/software: Hello! What is the recommended way to handle the PWRGD signal if the PWRDN functionality is not used? The datasheet states the following: "The first low-to-high transition of the PWRGD pin after device power is on…
Part Number: LMKDB1120 Other Parts Discussed in Thread: LMKDB1113 , LMKDB1112 , LMKDB1108 , LMKDB1104 , LMKDB1102 Tool/software: Hi team,
For below buffer, which can support power down tolerant? PDT stands for power down tolerance, which is usually…
Part Number: LMKDB1120 Tool/software: Hi TI team,
I would like to ask the Mid voltage on SDAR pin of LMKDB1120.
If i want to config 0xC2 address, TI suggest left float pin SADR1
But in the our old design with DB2000QL, we have a external voltage…
Part Number: LMKDB1120 Wistron re-done 3A validation for another motherboad, the same location, PLMKDB1120NPPR,
The engineers placed motherboard into inkwell, and then dry motherboard, engineer hard pull off this device from motherboard, result as below…
Part Number: LMKDB1108 Other Parts Discussed in Thread: LMKDB1120 Hi Team,
The customer observed that the LMKDB1120 saves 250mW of power when using a 1.8V supply.
They would like to know if there is data available for the 1108 and 1104 . Could you…
Part Number: LMKDB1108 Other Parts Discussed in Thread: LMKDB1120 , Hi Team,
The customer observed that the LMKDB1120 saves 250mW of power when using a 1.8V supply.
They would like to know if there is data available for the 1108 and 1104 . Could…