Part Number: LMQ62440-Q1 Tool/software: Can you provide an unencrypted spice model?
I tried to use the one that is on the web side for ansys EMC simulation, but it can not be use because is encrypted.
Part Number: LMQ62440-Q1 Tool/software: Please help provide the required data for the following table and attach the scanned documents of the IATF16949 certification. Thank you.
Manufacturer Name
Manufacture Part#
Part#
Description…
Part Number: LM62460-Q1 Tool/software: Looking for the unencrypted spice model for
LMQ62440-Q1
If I need to have an NDA, please let me know who I need to contact in order to sign one.
Regards,
Charles
Part Number: LMQ62440-Q1 Tool/software: Hi teams,
Does LMQ62440-Q1 has EMI report under the test conditions of V_IN = 24 V, V_OUT = 12 V, and multiple switching frequencies? Thanks.
Part Number: LMQ62440-Q1 Tool/software: Hi,
I'm trying to debug the fixed output 3.3V LMQ62440BPPQRJRRQ1.
It appears so far to operate appropriately when the enable output is on however there are a few issues with the off behaviour.
1. When…
Part Number: LMQ62440-Q1 Tool/software: I have integrated the LMQ62440-Q1 into a microcontroller board I am working on as the main power supply. The circuit I used is below and is pretty much exactly copied from the EVM schematic and the reference design…