Part Number: LMR14010A Regarding Eco-mode - I have a Vin of 6-9V, Vout of 5V, Iload of 50mA-600mA.
Light load conditions would be less than 5mA.
Can you tell me how the inductance value effects Eco-mode operation?
Inductance of 12uH: Will the LMR14010A…
Part Number: LMR14010A Hi all
My customer has a design using the LMR14010A, the specification is:
5V .... 32V => 3.3V/50mA, the device is mostly running in eco-mode.
They see a ripple of 40mV ... 60mV, which is too high for their application and is affecting…
Part Number: LMR14010A Hello,
I'm trying out something on LMR14010A. Is this device is suitable for variable output voltage? If don't use feedback resistor output voltage is variable?
Part Number: LMR14010A My design specification is: 5V input, 3.3V output, load typically in the range 350 to 400mA. Schematic as below.
I have this working on a number of boards, no problem. However on one specific board, the SW output never starts switching;…
Part Number: LMR14010A Hello,
I have used the LMR14010A in the past and it worked perfectly. However on a new design I have two LMR14010A's, one for 12VDC out and one for 3.3VDC output. The input voltage is 24VDC. The 3.3VDC output is 4.07VDC and the 12VVDC…
Part Number: LMR14010A Other Parts Discussed in Thread: LMR36015 Hello TI,
I have designed an IBB with LMR14010A. I used this application note as a reference.
Design is as follows:
-16.5V IBB Design
VIN
16.5
V
VOUT
-16.5
V
IOUT
0.5
A
MAX…
Part Number: LMR14010A Other Parts Discussed in Thread: TPS40305 , TLE2426 Hi
I am looking for regulator to conevert 10 -30V to 5V which goes to voltage reference. I need a regulator that have the least ripple and voltage swing when input voltage changes…
Part Number: LMR14010A Can a TI engineer confirm that the recommended operating temperature range for the LMR14010A is -40C to 125C? From the datasheet, the recommended range is -40C to 125C, but the absolute maximum range is "-0C" to 150C. I'm guessing…
Part Number: LMR14010A Hello,
I recently designed a board that uses the LMR14010a as a 3V3 regulator for powering a MCU from a 5-24V input. As of right now I haven't been able to get the device working and I'm not sure what's wrong.
The first…
Part Number: LMR50410 Other Parts Discussed in Thread: LMR14010A I have a question regarding LMR14010A and PLMR50410X
I’wondering what is difference between those two. In the Function block diagram I can see the PLMR50410X is much more complex, low side…