Part Number: LMR50410 Other Parts Discussed in Thread: LMR14010A I have a question regarding LMR14010A and PLMR50410X
I’wondering what is difference between those two. In the Function block diagram I can see the PLMR50410X is much more complex, low side…
Part Number: LMR14010A Hi,
Has LMR14010A used with inverting topology as below?
https://www.tij.co.jp/jp/lit/an/slva317b/slva317b.pdf?ts=1593156954964&ref_url=https%253A%252F%252Fwww.tij.co.jp%252Fproduct%252Fjp%252FTPS54060
Best Regards,
Kuramoc…
Part Number: LMR14010A Hi, Team.
could you tell me how much are the current limit_min and max ?
if we couldnt disclose it, do we have any devices which have specified min and max for current limit ?
LMR14010ADDCR
Part Number: LMR14010A I am trying to insert a circuit before the input of a SMPS circuit for following purposes
1) over-voltage and over current protection
2) EMC filter
3) resonance prevention
On above circuit,
Orange part has poliswitch for over…
Part Number: LMR14010A Other Parts Discussed in Thread: LMR16010 Hello everybody. I'm designing a buck converter (Vout=9V, Iout_max=0.5A), using the LMR14010A. As input voltage, I am using a 12V 7Ah lead-acid battery, and I want it to shut down the LMR14010A…
Part Number: LMR14010ALMR14010A
I followed the example schematic from datasheet, layout and installed the components.
the circuit output voltage is correct, but it can't load more than 1mA.
why?
Part Number: LMR14010A I am using this chip to convert 24VDC to 5VDC and provide power to DSP board.
DSP is used to generate PWM to drive a boost converter, and the PWM is isolated using a iso gate driver.
The gate driver power supply is also a isolated…
Part Number: LMR14010A Other Parts Discussed in Thread: LMR14020 Hi,
My customer asked for a 28-40v input and 24V1A output solution, we first recommend LMR14010A, but customer think the RθJA is a bit high(102℃/W), based on their experience, this device…
Part Number: LMR14010A Other Parts Discussed in Thread: LMR14030 , LMR14020 , LMR14006 , LMR16006 Tool/software: WEBENCH® Design Tools Hi,
I would like to use a LMR14010A buck switcher as converter from 10 V - 17 V to 3.3V, with max. current output of 0…