Hello,
Since we have not heard from you in a while I will be closing this thread. If you have more questions, please create a new thread.
Best regards,
Ridge
Part Number: LMR14050-Q1 Hi team,
For LMR14050SQDPRRQ1, when VIN1/VIN2 are 12V, EN=ON and FB pin becomes Open, what will be the status of output voltage?
Thank you,
Muwei Zheng
Part Number: LMR14050LMR14050 Switching Waveform as below,is this Subharmonic oscillations?
300mA load
1A load
I think LMR14050 have slope-compensation,and will not have Subharmonic oscillations,right?
Thanks!
Part Number: LMR14050 My customer was using LMR14050 for the below application:
Vin=24V, Vout=12V/ 2A.
They found the voltage output showed some unexpected ripple/spike during the soft start, with full load startup.
The issue was found if using the CC…
Part Number: LMR14050-Q1
Hello, can I use this circuit to enable/disable the LMR14050-Q1 through its enable pin? Basically when RESET_SIG is low, Q3 turns off. Do I have to put a pull-down resistor (R6 here) between the enable pin and GND?
Part Number: LMR14050-Q1 Hello
I am using LMR14050SQDPRTQ1 buck converter in my project in below specification.
Input-28VDC
Output-3.3V/5A
Issue- When I am increasing load 0.1A to upto1A then LMR14050SQDPRTQ1 has gone.
Part Number: LMR14050-Q1 Hi team,
I'd like to know PG pin output at Vin1:12V, Vin2: 12V, and EN=OFF(Low).
Customer expects PG:Low at EN=OFF.
Best regards,
Kento
Part Number: LMR14050-Q1 Hello,
I'm new to pspice and I've been trying to import the model for this part. Here's what I've done so far. >tools>generate part> selected downloaded LMR14050S_TRANS.lib file > create new part > Ok…
Part Number: LMR14050 Dears,
Customer use the LMR14050SDDAR with -10℃ and can not find the current vs temp data,could you pls kindly help to provide it?
Thanks