Part Number: LMR14050-Q1
Hello, can I use this circuit to enable/disable the LMR14050-Q1 through its enable pin? Basically when RESET_SIG is low, Q3 turns off. Do I have to put a pull-down resistor (R6 here) between the enable pin and GND?
Part Number: LMR14050-Q1 Hello
I am using LMR14050SQDPRTQ1 buck converter in my project in below specification.
Input-28VDC
Output-3.3V/5A
Issue- When I am increasing load 0.1A to upto1A then LMR14050SQDPRTQ1 has gone.
Part Number: LMR14050-Q1 Hi team,
I'd like to know PG pin output at Vin1:12V, Vin2: 12V, and EN=OFF(Low).
Customer expects PG:Low at EN=OFF.
Best regards,
Kento
Part Number: LMR14050-Q1 Hello,
I'm new to pspice and I've been trying to import the model for this part. Here's what I've done so far. >tools>generate part> selected downloaded LMR14050S_TRANS.lib file > create new part > Ok…
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 Hi,
Do you have any thermal models available for LMR14050-Q1.?
We would like to have ICEPACK model, since we are trying to have thermal simulations on Ansys.
Regards,
Arjun Udayakumar …
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 Hi TI support team,
I need a buck-boost power in my application.
Operating Condition: Vin = 9 ~ 16 Vout = 12V Iout = 500mA
I found a application note here https://www.ti.com.cn/lit/an/snva795…
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LM61495 , LM61460 , LMR14050 , LMR14020 Hi
We are using TI's Buck ICs for one of our projects with a automotive giant in US (for confidential issues we cant reveal the customer as well as project…
Part Number: LMR14050-Q1 Hi,
we have used this part for designing power supplies for one of our automotive application.
Can you review our schematics.?
Regards,
Arjun
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 Hi team
Cviauto use LMR14050 in IVI system for Bus (24V DC power), the power supply is battery, so the power efficiency at light load and standby mode must be paid attention to.
Could you…
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 , LM76005-Q1 , LM64460-Q1 , LM63460-Q1 I'm using the LMR14050-Q1 for our prototyping.
It seems that the sleep mode is activated due to the fluctuation of the current load, but this causes…