Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 , LM76005-Q1 , LM64460-Q1 , LM63460-Q1 I'm using the LMR14050-Q1 for our prototyping.
It seems that the sleep mode is activated due to the fluctuation of the current load, but this causes…
Part Number: LMR14050-Q1 Dear team,
My customer chose LM14050-Q1 to use as camera power supply chip.
They meets some issue and I want to ask you.
The input voltage range is 8.5~16V.
Output voltage is 8V.Loads current range is 1~2A.
Switching frequency…
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 Hello Guys,
Goo day.
Our customer is building a power supply using a LMR14050. What is the result if the SoftStart capacitor is left off and the SS pin floats?
The power supply is mains…
Part Number: LMR14050-Q1 Hello,
I would like to validate the selection of BOOT capacitor and series resistor for LMR14050SSQDDARQ1 device in my application by calculation.
The datasheet recommends 0.1uF/16V. But I would like to know the calculation behind…
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050 , LM61460-Q1 Hi Team,
My customer now use LMR14050 to convert 12V to 3.375V. The point of load(POL) in LMR14050 are BUCK and PMIC, which means that LMR14050 has two loads, BUCK and PMIC.
The …
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050
What is the voltage on a floating EN pin of a LMR14050? If it is V_in how do you know if it is an independent voltage or a short from V_in to EN?
Part Number: LMR14050-Q1 Other Parts Discussed in Thread: LMR14050
This question is a rerun. My original 5V power supply didn't work and I questioned why here on E2E. I concluded I had zapped the LMR14050 and replaced it with a new one. The new one…