Part Number: LMR16006 Dear team,
Customer use LMR16006, schematic as below, when BATT voltage>32V, LMR16006 failed when power on, vin=vout. When customer increase the output capacitor to 30uF, the fault will happen when BATT>40V. Customer must use 1uF…
Part Number: LMR16006 Dear sir/Madam,
We used "/SHDN" to adjust the system turn on voltage by using external resistors. According to the datasheet Ishdn = 1µA & Ishdn_hyst = 3.2µA @Tj=25°C.
The problem is that the datasheet…
Part Number: LMR16006 We are utilizing the LMR16006Y in a design to regulate a supply from 20-44V down to 15V.
Application load current is 118mA. Output capacitance is 41uF.
When power is first applied, the regulator switches at 172kHz-500kHz instead…
Part Number: LMR16006 Other Parts Discussed in Thread: LMR36006 I'm trying to lower my voltage from 15V to about 10.7V using LMR16006Y as my switching regulator. I used WEBENCH to preset a layout to go off on. Vmin being 14.25V. Vmax being 15.75 V. And…
Part Number: LMR16006 Hi,
I'm currently using the LMR16006 for one of my products. I'm interested in using it for another project, but a question was raised about the spectrum of the output voltage. I'm using the buck converter to power a sensor…
Part Number: LMR16006 Other Parts Discussed in Thread: BQ24040 , , TPS2553
Hi.
I use the TI webench to have a converter with the following parameters, 6.5 a 55 V as input, 5.5 V a 0.5 A as output. I am using the LMR16006X.
The output is connecting to a…
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: TPS54360-Q1 Hi Team,
LMR16006-Q1 and TPS54360-Q1 was used for customer project. It's a urgent case.
At first, they have some EMI issue, See detail information in attachment.
Customer decide…
Part Number: LMR16006 Hi, please could you tell me if it's safe to apply external voltage to the output of the buck converter with no input voltage?
I have added a diode in series with the input to prevent the reverse current flow, as recommended…
Part Number: LMR16006 I have a problem with LMR16006YDDCR. Input voltage is 12V, output voltage has to be 3,3V (I use resistor divider 33kOhm, 10kOhm at FB pin). But when I apply input voltage, output voltage is equal to 0,77V .(feedback voltage ??). Shutdown…