Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: LMR16006
Team,
-Are there any TI P2P dropped-in replacement available for LMR16006YQ5DDCRQ1 (LMR16006Y-Q1 in 5V fixed output) that does not require any PCB changes? -If not what would be the closest…
Part Number: LMR16006Y-Q1
Team,
Could you please provide the values of the internal resistors for the LMR16006YQ3 3.3V fixed output version? Are there some info on the appr, min/max of those values? Also could it be possible to share (offline if you prefer…
Part Number: LMR16006Y-Q1
Hi team,
Do you have DFMEA information for this device?
the background is customer use this device under 48V convert to 24V condition,
there are several defective devices under short status between Vin-SW.
if I use this device…
Part Number: LMR16006Y-Q1 Hello team,
my input range is 8 to 40V. I dont need an enable or shutdown funciton. Can I leave the pin floating or connect it directly to VIN? I would like to save some board space and not use a 100k pullup.
thanks for the…
Part Number: LMR16006Y-Q1 Tool/software: Hi TI team,
I am working on development board,in that i am using the fixed regulator IC LMR16006YQ3DDCRQ1.in that i implemented same circuit 3.3V as per the data sheet but i am not getting the voltage instead of…
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: TPS54360-Q1 Hi Team,
LMR16006-Q1 and TPS54360-Q1 was used for customer project. It's a urgent case.
At first, they have some EMI issue, See detail information in attachment.
Customer decide…
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: LM5166 , LMR16006 I've got a situation where my input parameters are fighting the design criteria. I know from reading that I actually need to use the LMR16006X part to have the lower 700kHz switching…
Part Number: LMR16006Y-Q1 Hi team,
LMR16006Y-Q1 min on time is 80ns, when the output is 3.3V/5V, how to make sure this can be done with 40V input voltage?
If not, when the output is 3.3V/5V, what is the max input voltage which can be supported?
Thank…
Part Number: LMR16006Y-Q1 Tool/software: WEBENCH® Design Tools Hi,
I have a customer who is installing the Webench connector in the OrCad and having an error when try to open the xml file.
Do you know what cause the error?
I have attached the screenshot…
Part Number: LMR16006Y-Q1 Hello Team, customer is missing some values in our datasheet to calculate quiescent current for worst case scenario:
- input current of pin FB (max. value over complete temperature range)
- max. Iq value over complete termperature…