Part Number: LMR23610-Q1
Hi,
I am using LMR23610-Q1 as follows:
Vin= 5.5 to 27 V
Fsw= 2 kHz sync with external clock
Iout = 0.4A
Vout = 5.5V
I am worried about what would happen at Vin_min = 5.5V. What would be the Vdrop across the IC and what Vout whould…
Part Number: LMR23610 We are using LMR23610 as a stepdown converter from 28V to 5.5V
We have had this design for a while.
But after time we got a new batch and get some problem.
To get the design running I have to change Vin from 28V to 17V and then…
Part Number: LMR23610 Hello,
We our using the LMR23610 in a product that has been in production approximately one year without any issues with this part. Recently we have had six units with erratic current draw during production testing. I have traced…
Part Number: LMR23610-Q1 Other Parts Discussed in Thread: LMR23610 , Hello Team, customer needs following configuration but seems it's not possible to do this with webench
I tried to optimize the LMR23610 Design with Webench Power Designer. Unfortunatelly…
Part Number: LMR23610 Hello,
I have been investigating this issue more. By increasing the inductance from 15uH to 22uH the current draw is stabilized. Reading the datasheet it shows that 15uH is recommended for 3.3V outputs. Attached is a schematic of…
Part Number: LMR23610 Hi Team
My customer is considering to use step-down converter LMR23610.
He has questions as follows.
Could you kindly help to answer? Thanks.
By checking the datasheet, I think the purpose of exposed pad and via on exposed pad are…
Part Number: LMR23610 Other Parts Discussed in Thread: LMR14006 , Hi team,
please tell us what type of behavior will IC do in case of current limit. (foldback ?) for LMR23610 and LMR14006
Part Number: LMR23610 Other Parts Discussed in Thread: LM5161 Hi Expert,
We would like to propose the LMR23610 for FLY-buck of isolated applicant.
Pls advice whether LMR23610 can support this FLY-buck design or not.
Thanks.
Best regards,
Eric Lai
…
Part Number: LMR23610 Hello,
In the LMR23610 data sheet, section 6.3 Recommended Operating Conditions, output current Iout is rated from 0A to 1A. The voltage regulator can source 1 amp on its output but can it also sink 1 amp?
Thanks
Part Number: LMR23610 Hi, Team.
I've been asked by Customer to know recommended value(L and Cout) for below required spec.
Vin:16.5V
Vout:5V
Iout:30mA
<Inductance>
As my calc, the below value looks ok but customer want to make sure how much…