Part Number: LMR23625-Q1 Tool/software:
Dear Team,
Since we are using LMR23625CQDDARQ1 buck regulator part of TI in our design. Understood from the datasheet is that the regulator supports input voltage range from 4V to 36V.
Requirement: Currently…
Part Number: LMR23625 Other Parts Discussed in Thread: TPS552872 Hey Buck Regulator Team,
I have a customer considering using the LMR23625 for a new project and we were hoping you could provide some feedback and design guidance.
The key requirements…
Part Number: LMR23625-Q1 Hi experts,
Let me confirm R_thetaJC in datasheet, please.
In the latest version (Revised_March_2018) shows 5.9C/W in DDA package. There is a big difference compared with past version value. Is this value correct? If it is…
Part Number: LMR23625 CTM find LMR23625 can only output current less than 1.7A(5V,continue). And IL will above 2A.
Attachment the SCH, pls help to suggest:
Part Number: LMR23625-Q1 Hi
Could you help to confirm whether the difference between LMR23625CFPQDRRRQ1 & LMR23625CFPDRRR is only in AEC-Q100 certification, thank you!
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMR23625 , LMR50410 Hi,
We are planning to use LMR23625 and LMR50410 in our design. Our input voltage range will be 9V to 36V.
The absolute maximum input voltage rating for LMR23625 and LMR50410…
Part Number: LMR23625 I HAVE 3 DIFFERENT POWERSUPPLIES FOR 3VDC, 4VDC AND 5VDC.REFER THE ATTACHED SCHEMATIC BELOW. I am facing issues which are as follows:
1. R67 & R69 HEATS UP AND BURNS ALONG WITH c42 OR C43 SHORTED.
2. R74 & R75 HEATS UP AND BURNS…
Part Number: LMR23625 In our device we have used the part LMR23625CDDAR as a wide input regulator which takes the input from the load dump protection circuit and then gives output to the battery charger IC.
for our compliance test we provide upto 36v…
Part Number: LM61430-Q1 Other Parts Discussed in Thread: LMR23625-Q1 , , LMR23625 Hi,
I would like to know what is the diffenence between LMR23625-Q1 and LM61430-Q1. I checked their specification and they seem to be similar, however, I am not sure if…