Hello Gareth,
The inductor current (channel 3) shows that the part hits current limit as expected and enters hiccup mode. After two cycles of hiccup mode the overload goes away and the output ramps back up. VOUT seems to pull up quickly and almost looks…
Part Number: LMR23625-Q1 Hi Expert,
My customer is using LMR23625-Q1 in the traction inverter, and having questions about the dropout mode. Can you help to answer?
When switching frequency started to foldback, what is the min limit switching frequency…
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMR23625 , LMR50410 Hi,
We are planning to use LMR23625 and LMR50410 in our design. Our input voltage range will be 9V to 36V.
The absolute maximum input voltage rating for LMR23625 and LMR50410 is…
Part Number: LMR23625 Hi team,
Our customer design an Inverting power supply with LMR23625C.
When the load current is over about 100mA, the current consumption is over 1A.
We share the schematic in the follow figure. Could you check the schematic and comment…
Part Number: LMR23625-Q1 Hi Experts,
Can you please help us to check what is the rising and falling time for LMR23625-Q1 internal high-side FET? My customer would like to verify the switching loss for this device.
Thank you.
Best Regards,
Wei-Hao
Part Number: LMR23625 Dear experts
For my low PCB budget design, I chose use the LMR23625, and I used the Webench.
I requite: Vin of 6.2v to 26.6v, with Iout=1.2A -(and 1.5A for short peaks)
The device is a 2.1MHz part- Efficiency is not of my main interest…
Part Number: LMR23625-Q1 I have the LMR23625CFQDDARQ1 installed and running but it drops frequency at low output. For another application I've used a different TI part that does maintain frequency under all conditions (TPS560430XFDBVR).
Is this normal…
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMR23625 , LMR36520 Hi
Does TI have pin to pin solution with LMR23625-Q1 but able to support Vin 60V?