Part Number: LMR23630-Q1 Other Parts Discussed in Thread: LMR23630 Hello TI experts,
my customer now tests LMR23630-Q1 because of the field issue.
They want to get simulation result to compare with the failure one.
I already did webench in TI site, but…
Part Number: LMR23630-Q1 About ESD Ratings spec as following screenshot, Q1 is just as same as non-Q1.
Could you please let me know the difference between JS-001 and JEP155/157 's standard?
Q1
non-Q1
Part Number: LMR23630-Q1 I am thinking of replacing "LMR23630ADDAR" with "LMR23630AFQDDARQ1".
"LMR23630AFQDDARQ1" is an in-vehicle grade product. What is the difference from "LMR23630ADDAR"?
Is it possible to replace…
Part Number: LMR23630-Q1 Hi Team,
My customer used LMR23630-Q1 for Auto traction inverter application, and reported very easy to damage while doing the soldering by handle. I've checked the AGND & PGND which is connected together outside, and the PCB…
Part Number: LMR23630-Q1 Hi all,
The continuous load current of the buck converter is written on the datasheet, I wonder how much limit of peak current that the device can survive?
For example, LMR23630-Q1 device can make continuous 3A.
However the…
Part Number: LMR23630-Q1 Hello all,
I could find min minimum 340kHz and maximum 460kHz switching frequency at 400kHz fixed frequency.
What is the meaning of min and max of fsw? Is this meaning the frequency can be changed from 340 to 460?
Can we calculate…
Part Number: LMR23630-Q1 Other Parts Discussed in Thread: LMR23630 Hi all,
The FB path layout goes near inductor, so I know that this noise and spikes came from the FB noise.
I know that FB noise makes a lot of problem on the stable output, but I cannot…
Part Number: LMR23630-Q1 Other Parts Discussed in Thread: LMR23630 Tool/software: WEBENCH® Design Tools Hello,
my customer has tried to run LMR23630-Q1 simulation at 2.1MHz Sync Frequency though, it could not. Because the Sync Frequency range support…
Other Parts Discussed in Thread: LMR14030-Q1 , LMR23630-Q1 Hello,
I want to know the smallest size of full version buck converter of LMR14030-Q1 and LMR23630-Q1 that we can make
Thank you!
Part Number: LMR23630-Q1 Other Parts Discussed in Thread: LMR23630 ,
Hi Team,
I have a question about LMR 23630-Q1.
Although it is equation (17) of a data sheet, I think that L is required.
I think the above equation is wrong. Is my recognition wrong…