Part Number: LMR33630 Can you give me a reference to how the equations in section 9.2 were derived? In particular, I am having trouble understanding section 9.2.2.4 equation 5 and section 9.2.2.5 equation 6. This applies to all the parts under the LMR336xx…
Part Number: LMR33630 Hi,
I want to use this buck converter to convert a 12V source to 5V. Do I need a snubber circuit? Is my schematic done correctly?
Best Regards,
Gil Abarca
Part Number: LMR33630 Hi team,
My customer wants to use LMR33630 for 20V/100mA max output. They want to use less capacitor for lower cost. For 2A situation, it's 4*22uF capacitance. And which value is suitable for 20V/100mA occasion?
Best Regards…
Part Number: LMR33630 I want to use this part "LMR33630". It also has all the technical documents to design the hardware. but I also need a WEBench Design tool simulation with all the graphs and BOM details.
unfortunately, simulation is unavailable…
Part Number: LMR33630 Hi everyone, I have a question about LMR33630.It has a maximum duty cycle=0.98, maximum input voltage=36V, but why the maximum output voltage is only 24V?
Part Number: LMR33630-Q1 Other Parts Discussed in Thread: LMR33630 Hi all
I found the LMR336 calculator from TI, I have checked from datasheet, but there is only one equation for Cout :
And when I try to do manual calculation, the result is different…
Part Number: LMR33630 Hi,
would you able to provide the gerber file for LMR33630ARNXT? If this is possible to share, I hope you can send it to my email.
Thanks!
Hi Prafulla,
There is no limitation on the input capacitor size, but the bigger input cap, the higher input inrush current, you need to consider the impact of inrush current and limit if necessary.
B R
Andy