Part Number: LMR36015 Hi TI expert,
The function of the capacitor between BOOT and SW is providing voltage for internal high-side driver. In the start time, If the high-side tube is turned on first, how does it turn on when the capacitor is no voltage? …
Part Number: LMR36015 I Use LMR36015 to realize the voltage conversion from 50V to 7.3V, but w hen I use "PSpice for TI" software for simulation, the total simulation time is 300ms, but when it reaches 100ms, the simulation is stuck and cannot be completed…
Part Number: LMR36015 HI there,
Does the industrial version of this part have Spread Spectrum? It's in the splash summary but I couldn't find it anywhere else in the datasheet? Looks like it could only be on the automotive part?
Thanks!
Part Number: LMR36015S Hi
The customer has a question they are testing the HOT-PLUG,
The voltage will exceed 60v and burn the LMR36015S ,
do you need to suggest adding hot swap?
Part Number: LMR36015S Figure 10-4 of the current datasheet shows efficiency down to 1mA.
Do we have any data for lower currents? We'd like to see 24V in, 5V out efficiency at 10uA load (or the equivalently, input/quiescent current under those conditions…
Part Number: LMR36015 We are currently using LMR36015BRNXR/BRNXT on our desings, When we change it to LMR36015FBRNXR/FBRNXT the power looses on the chip goes up by about 0.5W -
All we have done is just replace the chip on the board and left all other…
Part Number: LMR36015-Q1 Hi,
This is Regarding MPN -LMR36015AQRNXRQ1. Can you please provide the data for current (IVCC) corresponding to VCC. See the below snap.
Regards,
Ajay Sahu
Part Number: LMR36015-Q1 Hi team,
My customer want to confirm if this device can survive in Vout(not SW-pin but after LC filter) short to Vin(car battery) situation.
This device's FPWM option has negative current limit, so I think it's no problem. Could…
Part Number: LMR36015 Hi, I'm currently prototyping with a 1MHz non-forced part which powers a small MCU and is switched into a USB load via a low side NMOS switch. The MCU listens to the PG pin and if it receives a fault switches the USB out. On start…
Part Number: LMR36015 Hi,
My Requirement is 6V-36V Input, 5V Output, 1A Output, Ambient Temperature is (-40degC to 90degC). When I put this value in Webench Design tool for MPN-LMR36015 I got the the design In that design report for MPN-LMR36015FBRNXR…