Part Number: LMR36015-Q1 Hi team,
Which PACKAGE OUTLINE "RNX0012 B " or "RNX0012 C " is corresponding to "LMR36015AQRNXRQ1", which is shown in its datasheet?
Regards, Ochi
Part Number: LMR36015 Hi Team,
LMR36015 datasheet "10.2.1.2.9.1 External UVLO " describes "First, a value for RENB is chosen in the range of 10 kΩ to 100 kΩ".
Can we use lower RENB value like 1.6kΩ (< 10kΩ)?…
Part Number: LMR36015S Hello,
Could you please provide the Qualification Report of LMR36015SBRNXR ?
I asked CSC but they didn't have available data, and let me ask e2e.
Best regards,
Sakura Go/TED
Part Number: LMR36015-Q1 Hello,
We are using the LMR36015FSC3-RNXQ1 to generate 3.3V. Our client is requesting us to do measurements with failure injection. Among other, we have to test the open mode failure of the bootstrap capacitor.
I have desoldered…
Part Number: LMR36015 Other Parts Discussed in Thread: LMR33620 Hello,
A customer of mine is working on the LMR36015,
The maximum current they will want to use is 300mA, Once load current is low as 150mA they are seeing a decrease in the frequency –…
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36015 Hi!
I'm using a LMR36015FSC3RNXRQ1 in classic circuit configuration
Due the shortage of PMIC, we ar try to use a 3V3 regulator with feedback resistors, to obtain a 14Vdc required…
Part Number: LMR36015
Hi Team,
Good day. We have received inquiry from customer that there is an error in datasheet regarding the package measurement, kindly please confirm. Below is the details.
"
When determining the spacing between each of the…
Part Number: LMR36015-Q1 Hey All,
We had found one big problem during debugging LMR3605-Q1, as the theory, input voltage should equal to the output voltage, right? but when we rise the input voltage to 16v, output voltage can not be higher. The system…
Part Number: LMR36015 Hi Team,
it would be possible to receive the project of the DemoBoard LMR36015AEVM in Altium?
Or eventually the Gerber files of the same Demo?
Please,let me Know if possibile.
Thanks.Best Regards.