Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015FSCQRNXRQ1.
Can you please provide the current capability of Power Good (PG) Pin.
.Regards,
Ajay
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015FSCQRNXRQ1. The .lib file available in the website is not working for Ansys tool.
Can you please provide me the common .lib file which will work for every tool.
& One more thing that while simulating…
Part Number: LMR36015-Q1 Hi TI expert,
May I know whether LMR36015-Q1 has any OVP mechanism?
I notice we do have current limit and minimum on-time requirement.
So if the OVP do happen on Vout side, the controller will only reduce the PWM & frequency until…
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015AQRNXRQ1 . I tried simulating the circuit with PSPICE Model for following data.
Input - 6V-36V
Output - 5V, 1A
Switching frequency - 400KHz
I got some issues that while simulating I am getting…
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36006-Q1 , LMR36015 , LMR36006 , LMR36015S , We measure LMR36015FSCQRNXTQ1 case temp at room temperature and would like to find out if running it at 80°C ambient would maintain junction temperature…
Part Number: LMR36015-Q1 Hi,
This is Regarding MPN -LMR36015AQRNXRQ1. Can you please provide the data for current (IVCC) corresponding to VCC. See the below snap.
Regards,
Ajay Sahu
Part Number: LMR36015-Q1 Hi team,
My customer want to confirm if this device can survive in Vout(not SW-pin but after LC filter) short to Vin(car battery) situation.
This device's FPWM option has negative current limit, so I think it's no problem. Could…
Part Number: LMR36015-Q1 Hi team,
Which PACKAGE OUTLINE "RNX0012 B " or "RNX0012 C " is corresponding to "LMR36015AQRNXRQ1", which is shown in its datasheet?
Regards, Ochi
Part Number: LMR36015-Q1 Hello,
We are using the LMR36015FSC3-RNXQ1 to generate 3.3V. Our client is requesting us to do measurements with failure injection. Among other, we have to test the open mode failure of the bootstrap capacitor.
I have desoldered…
HI Richard,
I believe LMR36006-Q1 and LMR36015-Q1 has the same characteristics (except for output current capability), is it correct?
Is the LMR36015-Q1 400kHz CISPR data shown in LMR36015-Q1 datasheet?
Regards, Ochi