Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36015 Hi!
I'm using a LMR36015FSC3RNXRQ1 in classic circuit configuration
Due the shortage of PMIC, we ar try to use a 3V3 regulator with feedback resistors, to obtain a 14Vdc required…
Part Number: LMR36015-Q1 Hi Team,
We are facing issue with TI Webench while doing LMR36015A-Q1 IC Simulation with customized part data.
Webench stops to respond after entering custom part parameters and parameters are not updating on screen as well.
…
Part Number: LMR36015-Q1 Hi,
Is it acceptable to place a resistor in series with the capacitor between the Switch node pin 12 and Bootstrap pin 4? If so, up to what value 5 or 10 ohms?
There is a little noise from these supplies being picked up on an…
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36015 The datasheet states that the EN voltage "must not exceed the voltage on the VIN pin by more than 0.3V".
Would like to confirm this is under all conditions and is not just applicable…
Part Number: LMR36015-Q1 Hello Team, request from customer:
I wonder if I have chosen the right persons to ask in TI, I just assume the Switching Regulators
are under Power. The subject component is enrolled in our component database, and it is
categorized…
Part Number: LMR36015-Q1
Hi team,
I plan to apply 3.3V at VOUT when VIN=0V (reverse protection diode exist in VIN to Vbat) for debugging purpose(not normal condition)
(LMR36015-Q1 -3.3V fixed device)
Is there any concern in this condition?
1. Does the…
Part Number: LMR36015-Q1 Hi,
I am considering using the LMR36015-Q1 device. I would like to ask you about the inductor selection. The specifications are as follows.
(question 1) I first calculated the inductor with a permissible current of 1.5A for this…
Part Number: LMR36015-Q1 Hi team,
My customer would like to know power dissipation of LMR36015AQRNXRQ1 with below condition.
Could you support this request?
- Vin : 15Vmin to 58Vmax
- Vout : 12V
- Iout : 0.4A
- Fsw = 400kHz
- L = 140uH
I tired to estimate…
Part Number: LMR36015-Q1 Hi, Good day. I hope you are doing fine. Our customer wants to use the LMR36015-Q1 in their ECU and he has a question regarding the inductor value for his design. They intend to use this to step down the 24V to 12V/1.5A, 400kHz.…