Part Number: LMR36015-Q1 Hi team,
My customer would like to know power dissipation of LMR36015AQRNXRQ1 with below condition.
Could you support this request?
- Vin : 15Vmin to 58Vmax
- Vout : 12V
- Iout : 0.4A
- Fsw = 400kHz
- L = 140uH
I tired to estimate…
Part Number: LMR36015-Q1 Hello, I am currently working on bringing up a PCB we have designed with a LMR36015-Q1 being used to convert 36V to 5V.
Unfortunately, the converter is not working properly. When 36V is applied, the converter appears to be stuck…
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: DRV8872-Q1 , Hi there,
Is there a specified value for the maximum current capability of the integrated MOSFETs body diode?
Best Regards,
Christian
Part Number: LMR36015-Q1 Hi team,
In datasheet an input supply current (ISupply) of 26µA is stated on page 8. Diagram on page 33 is showing a graph from 19 up to 32 mA(!). Which one(µA, mA) is correct?
Best Regards, Tom Liu
Part Number: LMR36015-Q1 Hello Team,
I would like to understand what Delta Vout means in the following equation:
The datasheet says, "output voltage transient". Does that mean if I want the output voltage to deviate by less than 50mV during a load transient…
Part Number: LMR36015-Q1 Hi TI-team
My customer want 3.3V of Switching Frequency vs Input Voltage.
They use Vin:32V, Vout=3.3V, Freq=2.1MHz
I think under the above conditions it will be less than Min On-time.
Min On-time is 49.1ns @Vin:32V, Vout=3.3V…
Part Number: LMR36015-Q1 Hey there
I have a problem with the simulation/model of the unencrypted LMR36015FSC-Q1. I always get an error, when i try to simulate it.
At first I created the schematic on my own. Afterwards I downloaded the done schematic…
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR33620-Q1 , , LMR36015 Hi Team,
Is it acceptable to setup an external UVLO circuit for the LMR36015-Q1? I see that in the LMR33620-Q1 datasheet, I see that it is acceptable via section 9.2.2.10…