Part Number: LMR51610 Other Parts Discussed in Thread: LMR51606 Hello guys,
One of my customers is interested in LMR51606, 0.6A version of LMR51610.
At this moment, they have the following question. Could you please give me your reply?
Q. When is LMR51606…
Part Number: LMR51610 Other Parts Discussed in Thread: LMR51450 , Hi Team,
When you look at the library model of LMR51610 in PSPICE it has a description of LMR51450. Can you confirm the library model in LMR51610 PSPICE model is for LMR51610?
If it's indeed…
Part Number: LMR51610 Other Parts Discussed in Thread: LMR50410 Hello,
I would like to use the LMR51610 in Inverting Buck-Boost configuration, to build a DC/DC converter with the following specs:
Vin = 24V +/- 10%
Vout = -15V
Iout = 0.5A max
This would…
Part Number: LMR51606 Other Parts Discussed in Thread: LMR51610 Hi team, I'd like to know the efficiency vs load current data for the LMR51606. Should I use LMR51610 instead? BR, Kengo.
Hi David,
I was introduced to a similar product, LMR51610, in another thread. Therefore, I am simulating the LMR51610, but an ERROR (ORCAP-15089) occurs and I cannot perform the verification. Can I get any comments?
Thanks,
Hi Shuji
What is the input source and will the Vinmax>24V ?
Will customer take a look at TPSM5601R5H ?
If customer consider using converter, I would recommend LMR51610 . There is also an apps note for LMR51610 operating as inverting buck boost.
Thanks and…
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: LMR16006 , LMR51610 , LM5164-Q1 , LMR36503-Q1 Hi,
I would like to use the LMR16006Y-Q1 for IBB application.
VIN = +12V, VOUT = -24V.
What is the leakage current of the Feedback pin?
What is the maximum…