Part Number: LM2672 Other Parts Discussed in Thread: LM22672 , TLVM13620 Hi to all,
I have a question regarding the LM2672MX-ADJ/NOPB.
As there are supply issues with this part and with all fixed voltage derivates!!
Is there a possible P2P replacement…
Part Number: LMR50410-Q1 Other Parts Discussed in Thread: LMR50410 , LMR54410 What is the minimum MS Office requirement to run LMR50410-Q1 Quick Start Tool.xlsm and LMR54410-Q1 Quick Start Tool Final.xlsm?
LMR50410-Q1 Quick Start Tool (sluraz6.zip): LMR50410…
Hello Gencay,
The commercial device's (without automotive qualifcation/guarantee (-Q1)) tend to be lower in cost.
If you only need operation up to 36V and don't need automotive qualification, then, I would advise:
OptA
LMR54410
OptB
LMR36503 …
Part Number: LMR14010A Other Parts Discussed in Thread: LMR54410 , , MC34063A Dear Sir/Madam,
I have a question about LMR14010A and LMR54410 :
Is it possible to vary the Voltage Output adding an Offset on the FB of DC-DC's Input through an OPAM? Ishow…
Part Number: LMR14010A Other Parts Discussed in Thread: LMR54410 , LM5158 Hi all,
I've been testing LMR14010AEVM Evaluation board and I have a trouble. I've modified PCB for VIN=35V, Vout=27V/750mA, Cout = 4.7uF x2 + 100nF
With Resistive Load is…
Is there a specific Vinmax that you need for any ringing or headroom? It sounds like 18V +/- 20% would be covered by a 24-28V device.
The TPS62175 is a 28V 0.5A device that should work for your specs
LMR54406 (36V; 0.6A) is one of our newest devices and…