Part Number: LMR66430 Tool/software: Hi Team, I am calculating Enable resistor calculation for the LMR66430R5RXBR for the project. but web bench result is differed from my calculation. can you please share the calculation excel file for the same.
…
Part Number: LMR66430 Other Parts Discussed in Thread: LM5169 , LM5168 Tool/software: Hi Sir,
My customer would like to use LMR66430R5RXBR(operating freq at 2MHz) to pass the ISO7637-2-Pulse 2a test.
They will add a 58V EMI/EMC protection component…
Part Number: LMR66430 Tool/software: Hi Sir,
May I know there have any efficiency curves for operating frequency at 1.7MHz? the datasheet only provide the curves for operating frequency at 400KHz.
Part Number: LMR66430 Tool/software: Hello, I would like to request an unencrypted SPICE model for part number LMR66430. I am not sure if this is the best place to ask, but I was hoping someone might be able to point me in the right direction. Thank you…
Part Number: LMR66430 Tool/software: Hello TI engineers I have a question about LMR66430MC5RXBRQ1.
I am using WEBENCH POWER DESIGNER to use this IC with external synchronization. I have entered the input and output conditions and pressed the “VIEW DESIGN…
Part Number: LMR66430 Tool/software: We designed several power supplies with TI chips. There were always Webench simulations, which allowed us to prove our designs and then they worked just out of an assembly house. All chips were with fixed 400 kHz frequency…
Part Number: LMR66430 Hi
My customer got an requirement that under the conditions Vout = 3.3V @ 250uA or 5V @ 180uA , the current of
Vin 12V need below 100uA.
May i check if LMR66430 can meet this requirement? thanks !
Part Number: LMR66430 Tool/software: Hello
Could you please let me know IC's which can work upto -55degC and can handle current of about 30Arms for AC/DC, DC/DC conversion?
It can be any topology: example, buck/boost/buck-boost or flyback or forward…
Part Number: LM62460 Other Parts Discussed in Thread: LMR66430 , TLVM14406 , TLVM23625 Tool/software: Hello team,
I'm creating the design with the condition, Vin:24V / Vout: 2.3V / Iout :2A.
If I use LM62460, Webench is warning about minimum On time…