Part Number: LMS3655-Q1 I am checking MTBF for the LMS3655MQURNLRQ1.
The default output shows 0.1 FIT and 7.01xE9 MTBF, however when i tried calculating for a different temperature, i noticed that if i put 55c, i need to set FIT to around 0,1426 in…
Part Number: LMS3655-Q1 Dear Sir,
My customer would use LMS3655-Q1 to design a infotainment(10V~36Vin, Vo=4.2V/5A).
have a key spec: light load eff >80%during Vin=36V Io=4.2V/8mA
He have a confuse: he saw datasheet fig24 eff. curve basic can meet…
Part Number: LMS3655-Q1 Hi support team,
I wanna confirm Ta (MAX). It is different between "ROC" and "PACKAGING INFORMATION". Which one is correct?
Page-5, SNAS714C
Page-49-50, SNAS714C
・・・
Regards, Dice-K
Part Number: LMS3655-Q1 Hi support team,
I wanna confirm Ta (MAX). It is different between "ROC" and "PACKAGING INFORMATION". Which one is correct?
Page-5, SNAS714C
Page-49-50, SNAS714C
・・・
Regards, Dice-K
Part Number: LMS3655-Q1 Hi team,
Does LMS3655-Q1 have a low-voltage output mode?
I have one question at using Vin < Vo .
If Vin=5V, Vo= 5.5V
When the input is reduced to 5 volts, can the output be set to 5.5 volts and output? If 5V is input, what…
Part Number: LMS3655-Q1 Tool/software: WEBENCH® Design Tools When simulating LMS3655AQRNLRQ1 in WEBENCH with Vout=5.05, 4.5A then the minimum allowed Vin is 6.7V. According to the datasheet it should be around 5.5V.
Why is the VinMin so high in WEBENCH…
Part Number: LMS3635-Q1 Other Parts Discussed in Thread: LMS3655-Q1 Hello, Could you kindly introduce typical application schematic if I use below 3.3V output ? The background to this question lies in note(3) of section 7.3 in the LMS3655-Q1 datasheet…
Part Number: LMS3655-Q1 Other Parts Discussed in Thread: LM73606-Q1 , LM73605-Q1 Tool/software: WEBENCH® Design Tools Hi Team, My customer considers to use LMS3655-Q1 for the following automotive application. ---------------------- Vin: 18 - 36V *ABS…
Part Number: LMS3655-Q1
Dear Team,
we received a request if it was possible to do a frequency sweep with the external clock.
The customer has a requirement only allowing a DC/DC switching frequency lower than 300KHz. This frequency is only possible…
Hello,
You can refer to the device datasheet for the pre-regulator and PMIC which will provide all of the details on these parts.
LMS3635-Q1 3.5-A, LMS3655-Q1 5.5-A, 36-V Synchronous, 400-kHz Step-Down Converter datasheet (Rev. C) (ti.com)
LP87702…