Part Number: LMV761 Other Parts Discussed in Thread: TLV3501A-Q1 , TLV3501 Hi Team: The Datasheet of the LMV761 says: ‘Voltage between any two pins not more than Supply Voltage’ and ‘Current at Input Pin ±5 mA’ But it says…
Part Number: LMV761 Dear E2E member,
I want to know the differential input which is IN+ - IN-, the maximum rating is 5.5V, right?
Is it OK for this design as below?
Part Number: LMV761 The data sheet ( SNOS998I – OCT 2015) specifies a typical value for Ton (Turnon time from shutdown) for various conditions.
Is Ti able to provide a (max & typ) figure for the time from shutdown (/SD) failing to the output…
Part Number: LMV761 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I need to get the spice model for the LMV761 and import it into the TINA-TI simulator. This comparator has a shutdown pin which I need to be part of the…
Part Number: LMV761 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I am using an LMV761 Spice model provided by TI and I am seeing something in the simulation I don't understand. My application uses a 5V supply for the…
Part Number: LMV761 Hi, My question is about how to consider the Common-mode input-voltage range of the LMV761. The datasheet gives a CMVR equal to 3.8V when the component is supply with 5VDC. In my application V- = 0 to 5V and V+ = 0,5V. Defintion of…
Other Parts Discussed in Thread: LMV761 , LM339 , LMV331-N Hello TI,
If someone can answer whether for LMV761 if an input is close to the VICRmin (-0.3V) and the other is 0V what happens with the bias currents? Are they still in the pA range or do they drift…
Other Parts Discussed in Thread: LMV761 Britt-
Now, I am working on a new circuit that has a slot for the LMV761.
Your 'open' Spice model does execute in LtSpice, however some of output results seem unusual when operating within the new design.…
Other Parts Discussed in Thread: LMV761 I'm thinking of using LMV761 comparator for Si PIN photo diode ( Vishay VBPW34FAS ) input circuit for serial communication.
To get the maximum speed from the photo diode, I want comparator with very low input…
For logic gates, the switching thresholds are not very well specified.
Consider a relaxation oscillator with a comparator ( SNOA998 ). This is the same circuit as above, but the additional voltage divider sets a more precise threshold. The LMV761 has a…