Part Number: LMZ12008 Dear Ladies and Gentlemen,
I have a pcb according to your design, but found out that the LMZ12008 is not outputting the 5 Volts requested, but a lot less voltage. I used tried the following resistor configurations without luck: R_ffb…
Part Number: LMZ12008 HI
I am designing a DC-DC buck where Vin= 12V, Vout=5V/5A with 0.1% load regulation. I am using LMZ12008 and design with web-bence. But in reality I am not getting 0.1% (5mv) load regulation at 5A, Voltage drops down to 4.884V.
…
Other Parts Discussed in Thread: LMZ12008 , LMZ12002 , LMZ12003 Hello,
Am using LMZ12008 IC With En pin will be driven by MAX16009 voltage monitor open drain ic.
What is the Sink current for EN pin to driven low.Can this MAX16009 IC able to sink ?
Regards…
Other Parts Discussed in Thread: LMZ12008 Hy everybody! I want use the LMZ12008 with 6V and 4A on the output. I counted the output voltage, that is ok. But I can't set the current. How can I do? I used Cout=470Uf and 140Uf=Cin.
Hi,
I would like to understand how adding Cff would improve anything on page 3.... There is no mention to this capacitor in the rest of the datasheet
Yo
Other Parts Discussed in Thread: LMZ12008 I'm having some trouble understanding how to set the UVLO thresholds for the LMZ12008 module. Looking at the data sheet , page 15, the example gives R ENT = 42.2kΩ and R ENB = 12.7kΩ, for "a rising UVLO…
Other Parts Discussed in Thread: LMZ12008 Design Parameters: Vin: 14V DC / Vout: 5.2V DC / Iout: 4.2A / Ta: 50degC / Max Tj: 100degC / 2-layer PCB
Interpolating between Vin of 12V and 16V, and between Ta of 25degC and 85degC on the LMZ12008 …
Other Parts Discussed in Thread: LMZ12008 We seem to be having a lot of trouble successfully manufacturing PCB assemblies on which the LMZ12008 is a component. The assembly is being manufacturing in a lead free process that we have successfully used for…
Has anybody tried pushing the output voltage up on the LMZ 12008?
I am currently running one at 8.45V @ 6A and it seems to be running just fine (12V input).
Will I run into problems over the long term?
Is there a limit? (everywhere I read it says 6V,…
Other Parts Discussed in Thread: LMZ12002 , LMZ12008 , LMZ23610 , LMZ22010 HI,
To increase output current, is it possible to cascade LMZ12008 and LMZ12002 ?