Part Number: LMZ12010 Hi,
Our team have some queries here in regard our finding upon do CSAM to this ICs. During x-ray, we observed some voids inside this ICs.
After using 100x scope and focusing to this void area, we found that these voids are actually…
Part Number: LMZ12010 Hi,
We have built a lot of 10 PCBAs. 4 seem to exhibit a strange failure: 5V output does not come up, and all 4 PCBAs have pins 7 (FB) and 8 (SS) shorted. one of the PCBAs also has VOUT and GND shorted.
Verified short is inside…
Part Number: LMZ12010 Tool/software: WEBENCH® Design Tools When changing the "Enable UVLO Option" from "Basic design" to "UVLO enabled design" in the "Configuration Options and applying it by pressing "Redesign", the website refreshes but the changes…
Other Parts Discussed in Thread: LMR64010 , LMR62014 , LMZ12010 , LMZ34002 , LMZ31710 Hi ,
I want to generate 28V/0.5A , 24V/0.2A , 15V/3.2A , 12V/1A , 8V/2.7A , 5V /7A , 3.3V /9A , -5V/1A . Input voltage is a battery Liion range : 6V-9V .
For output voltages…
Hello Kent,
TPS84A20 is 100% compatible with LMZ31710.
You may also want to consider LMZ22010 , LMZ12010 , PTH08T241W , PTH08T240W .
I am not an expert in supply chain issues, so I will refrain from trying to explain the reason for the shortage.
Happy holidays…
Other Parts Discussed in Thread: LMZ12010 Hi everyone,
We tried to solder the LMZ12010 Simple Switcher by hand, but afterwards, we found that the VOUT and AGND pins were shorted inside the IC. We think this is because we made lots of mistakes in soldering…
Other Parts Discussed in Thread: LMZ22008 , LMZ12010 Dear Sir/Madam,
I have a PCA that uses 4x LMZ22008 and 1xLMZ12010. A high failure rate has been observed on the LMZ22008 (approx 40%). A low failure rate has been observed on the LMZ12010 (approx 5%).
The…
Other Parts Discussed in Thread: LMZ12001 , LMZ12010 , TPS3700 , TPS386596 Hi Sir / Madam ,
This vengat here from Avnet , one of my customer selected the LMZ12001 , LMZ2208 , LMZ12010 , MZ12003 for telecom application . customer would like to get the Power…
Other Parts Discussed in Thread: LMZ22010 , LMZ23610 , LMZ12010 , LMZ13610 Can the LMZ22010 or LMZ23610 be using in an inverting configuration with current sharing? If so, is there any level shift that must be perofrmed on the current share line?