Part Number: LMZ13608 Hello - is there an upper limit on the Renh resistor? We would like to increase the hysteresis to > 1V. So could I use a 100kOhm without issue? Renb = 10kOhm and Rent = 63.4kOhm (9.35V enable).
Thank you.
Brett
Part Number: LMZ13608 Hello,
LMZ13608TZE still has problem like CS0481694 , I couldn't find what is the problem.
If we send my whole Board Can you check what 's the factor has caused problem on my board? I am looking for your reply.
Thanks
Part Number: LMZ13608 Hi Team,
Our customer would like to request a schematic design review of their application using 4pcs. of LMZ13608. Please refer to the schematic diagram below.
LMZ13608TZ_NOPB 검토 회로 (1) (1).pdf
Regards,
Danilo
Part Number: LMZ13608 Hi team,
the customer have a question:
LMZ13608TZE/NOPB.
The product was produced using the circuit diagram and product that you advised me. Shorts occur at pins 6 and 7.
Please check what is the cause of the short circuit.
At our…
Part Number: LMZ13608 I tried to set UVLO and hysteresis based on the figure 48 of the data sheet. I am using 56K for RENT, 5.6k for RENB and 2.2k for RENH.
Measuring the circuit I found that I do not get the expected values for the threshold and hysteresis…
Part Number: LMZ13608 Hello,
the LMZ13608 emits a high whistle tone. It is the coil onthe module. (Vin 12 V, Vout 5V, Iout 4 Amps. What can we do about it?
best regards
Norbert Brendle
Part Number: LMZ13608 These parts are used by us on test equipment used to test deliverable hardware. The customer for the deliverable hardware needs a definition of possible failure modes and mitigations to those failure modes which would cause or allow…
Part Number: LMZ13608 Hi engineers,
I'm planning to use LMZ13608 for my supply board. I would like to confirm layout recommendation for thermal vias indicated in the datasheet.
Is this really diameter or are you referring to the drill size?
If it's…
Other Parts Discussed in Thread: LMZ13608 , LMZ14203H Dear all,
I want to set output voltage of LMZ13608 to 7V .
The load current is less than 2A.
Can I set to that?
Sorry for the long long delay…
Is the LM25116 also a good solution for a Load with a variable current need. The current need changed very slowly between ~7-16Ampere.
Or are there a better solution?
Thanks a lot!
Mathias