Part Number: LMZ35003 Other Parts Discussed in Thread: LMZ13608 To Whom It May Concern,
Please let me know about the latest temperature profile of LMZ35003.
According to the datasheet link, the following file is the temperature profile.
[Data Sheet…
While it is technically possible to parallel two modules, it is generally not practical. If you need more current what not look at LMZ13608 up to 8 A power module?
Other Parts Discussed in Thread: LM26003 , LMZ13608 , LMR14050 , LMZ14203 , LM53603 , TPS54560 , TPS54561 , TPS54540 Hello, I want to use the LM26003 for a design with a GSM / GPRS modem. The application is suitable? peak current required to 30mA to 3A PWM / fPWM…
Other Parts Discussed in Thread: LMZ13608 , LM3150 I am working on a design using an LM3150 to take 10v-30v and produce 5.25v out at anything between 0.5A to 5A depending on user needs. Essentially using Webench to do most of the hard work in terms of the…
Almost any Simple Switcher with an 8A rating could be used; like the LMZ13608.
Paralleling two converters requires special care and I would avoid doing that.
FD
Other Parts Discussed in Thread: LMZ23608 , TPS2113A , LMZ13608 , TPS3700 Hello,
We are considering using two LMZ23608's in parallel (5V out), but are doing so to use them as redundant supplies (safety critical).
In the design notes the slave supply doesn…
Other Parts Discussed in Thread: LMZ13610 , LMZ13608 Hi,
We have done a design using LMZ16308 voltage regulator for powering a cell phone module Cinterion TC 65 inside a small unit that coexist with GPS (GNSS) receiver RTK high precision. The problem we…