Part Number: LMZ14203H Hi All,
I am thinking of using LMZ14203H as buck module to convert from 24V to 21V. To have some design margin for the front end loss, I want the design to be able to work at 23.5V. When using the power designer for simulation…
Part Number: LMZ14203H Hi All,
I am thinking of using LMZ14203H as buck module to convert from 24V to 21V. To have some design margin for the front end loss, I want the design to be able to work at 23.5V. When using the power designer for simulation…
Part Number: LMZ14203H Hi All,
I am thinking of using LMZ14203H as buck module to convert from 24V to 21V. To have some design margin for the front end loss, I want the design to be able to work at 23.5V. When using the power designer for simulation…
Part Number: LMZ14203H Tool/software: I have a very strange problem with the circuit in the attached drawing.
The Vin is 18-30VDC, nominal 24VDC and the required output Vo 14.2V.
The UVLO is set at 16.2V. Output capacitors are all ceramic . The load…
Part Number: LMZ14203H Tool/software:
Dear TI Technical Support Question: We have decided to use the LMZ14203H and are designing a circuit. The specifications are as follows. Input voltage: 14V Output voltage: 12V Output current…
Part Number: LMZ14203H Tool/software: I am writing to request your assistance with a technical query regarding the LMZ14203H regulator.
I am currently designing a power supply and need to implement a shutdown function for the regulator. I have reviewed…
Part Number: LMZ14203H Tool/software: Hi Team,
I am using LMZ14203HTZ/NOPB to convert VIN=12V to VPUT=5V and as per the data sheet VIN (8-42v) , COUT 100KOhm bigger in package size.
Additionally RON=100KOhm, RFBB=6.49KOhm, RFBT=34KOhm.
Can you…
Part Number: LMZ14203H Other Parts Discussed in Thread: LM22670 , LMZ14203 , LMR38025-Q1 , LM70840 , LM76003-Q1 , LMR36015S Tool/software: I am using the LMZ14203H where the input is 24V - 36V and the output is 5V. this part has successfully passed our…
Part Number: LMZ14203H Tool/software: I'm trying to understand what TI controller is used in the LMZ14203H simple switcher. The controller in this switcher has a problem with transient response when it transitions from continuous to discontinuous mode…
Part Number: LMZ14203H
Hello Support,
We are currently using the LMZ14203H to convert a +32V DC input into an 18V DC output. Our +32V bus maintains a steady state within a range of +/- 3%, although in emergency situations, it has the potential…