Part Number: LMZ23605 Hello,
Is the LMZ23605 suitable for Vapor-Phase Soldering (VPS)?
Currently we are using Würth Elektronik 171050601 which is pin-compatible to the LMZ23605. Our problem is that the Würth Part 171050601 is NOT compatible with VPS…
Other Parts Discussed in Thread: LMZ23605 Tool/software: We are using the LMZ23605 with 12V in and set up for 3.3V out. Our application is for 3A max load on output.
We had a failure of this part in our application where the output (pin 7) appears to…
Part Number: LMZ23605 Tool/software: Dear Sir/Madam,
We want to use LMZ23605 DC-DC Converter for new design. Please provide the life time and also mention is it recommended for New deign,Active or not.
And also suggest the Isolated and Non-Isolated…
Part Number: LMZ23605 Tool/software: Hello,
I want to use the LMZ23605TZ as a -5V output.
I am not planning on using the synchronization Input. Should I connect this input to AGND or leave it floating?
Thanks,
-Tal
Part Number: LMZ23605 Other Parts Discussed in Thread: LMZ14202 Tool/software: Equation (5) used to calculate Cfb does not reconcile with the values obtained in the two design examples: Ex1 LMZ23605 Cfb = 2.5 uF and Ex2 LMZ14202 Cfb = 6.4 uF. The calculations…
Hi Juan,
I recall you mention you had 2 of these devices on 4 different boards so a total of 8 LMZ23605 circuits with all undesirable output.
I don't suspect the LMZ23605 device to have manufacturing issues since the part has been in the market for…
Part Number: LMZ23605 Other Parts Discussed in Thread: LMZM33606 I require a negative output from LMZ23605(-5.5V),but the chip give me a unstable -1.2V output(I can't use the -1.2V because it varies from -1.21 to -1.23 and never stop),my design is like…
Part Number: LMZ23605 The operating temperature range specified in the data sheet is -40°C to +85°C, and the junction temperature range is –40°C to +125°C. I need maximum operating temperature up to +125°C. Do you have any other suggestion for the LMZ23605…
Part Number: LMZ23605 Hi,
I ask you about the latch-up of the LMZ23605. This device has passed the latch-up test under the conditions specified in JESD78.
Question 1 If current or voltage stress exceeding the conditions specified in JESD78 is applied…