Part Number: LMZ23608 Tool/software: Dears,
to support our RD team, we need a 3D model of the LMZ23608. We see having this essential for proper thermal management. Unfortunately, only ffotprint data is available on the TI.com, not full 3D model.
Part Number: LMZ23608 Hello,
We experienced a failure of a LMZ23608TZ and would like to learn more about common failure modes of this device. Our LMZ23608TZ IC heated up, cracked, and shot solder all over our board. We have pictures we can provide given…
Part Number: LMZ23608 Hi team
Could you tell how many LMZ23608s can be used for current sharing?
Customer wants 3pcs of LMZ23608. Is this possible?
Regards,
Noriyuki Takahashi
Part Number: LMZ23608 Hello Guys,
Good day.
Customer downloaded the TI PSpice model for LMZ23608 with the hope of configuring two in parallel (master/slave configuration). Apparently, the model does not permit that important feature. What options does…
Part Number: LMZ23608 Other Parts Discussed in Thread: LM2842 , Hello,
I am using four LMZ23608 in current share mode in my design in order to supply a high number of addressable LEDs. The microcontroller which generates the input signal to the LEDs is…
Part Number: LMZ23608 Hi.
We are using this IC for our application.
And our use case is 24 Vin to 3.3V Vout @ 8A load.
As per the datasheet's thermal derating curve, the max load current for thetaJa 9.9 degC/W is around 6A for the ambient temperature…
Part Number: LMZ23608
I would like to get the junction-to-case (bottom) thermal resistance for the LMZ23608TZE/NOPB during natural convection conditions. The data sheet lists junction-to-case (top) and junction-to-ambient but does not list the junction…
Part Number: LMZ23608 Does TVS diode necessary for LMZ23608 design? Is transient-voltage-suppression built in LMZ23608?
If constant input voltage goes over 36V, is there any input voltage clamping mechanism in LMZ23608?
Part Number: LMZ23608 Hi!
We have chosen LMZ23608 module for speeding up our design. Input voltage: 11 ... 21V. Output Voltage: 5V. Max output current: 6A. I think it will all work fine. We have only one concern. Our minimum output current can be as low…
Part Number: LMZ23608 I have been using LMZ23608 as voltage regulator for one year and I get very good results. I have been using a Voltage constant control mode by RFBT and RFBB, but I wonder If I could use a Power constant control mode leaving unmounted…