Part Number: LMZ31520 Hello
I need the temperature derating curves for Junction temperature.
The data sheet only contains Ambient temperature information.
Regards.
Part Number: LMZ31520 Other Parts Discussed in Thread: TPS53355 Can you tell me what the unity gain is on these two parts. Marvell uses a TPS53355 part with a feed back loop to keep the voltage level stable at the switch chip. Their application note says…
Part Number: LMZ31520
Hi,
I have designed a board with LMZ31520RLGT.
The schematics part is as below
Please let me know if anything I have missed out here.
We are observing a 1.92V on the output, we have checked the resistor before mounting and its 324E…
Part Number: LMZ31520 Hi!
Help me please with one question on LMZ31520.
Is it still possible to have power-good functionality on the PWRGD pin while using Forced Continuous Conduction Mode? I.e., is it correct to have the PWRGD pin pulled up to V5V pin…
Part Number: LMZ31520 Other Parts Discussed in Thread: LMZ31530 Hi, Could you tell me about LMZ31520/30 high and Low side SW Rds(on)? My customer is considering LMZ31520 and LMZ31530. Customers plan to adopt LMZ31530 when the load current increases. However…
Part Number: LMZ31520 Is there efficiency data of below condition for LMZ31520?
⇒PVIN:3.3V、VIN:5V、Vout:1V、Iout:~20A
※Datasheet is described only PVIN:3.3V、VIN:5V、1.8Vout.
Webench can't simulate PVIN:3.3V condition.
Best regards,
Satoshi
Part Number: LMZ31520 I could not find information about Thermal pad size(dimension) in datasheet and foot print information.
Please, I need thermal pad size.