Part Number: LMZ31710 Hi,
Kindly seek your help to advise the correct body marking for MPN: LMZ31710RVQR.
As in the datasheet, the part marking should be (54020, LMZ31710). Hence, w e would like to know does below part marking image denotes to the…
Part Number: LMZ31710 Hi TIer
My customer use LMZ31710 in many project.
My customer use 80 pieces of the LMZ31710 on a new project and found that 30 pieces have no output. We discovered that the Vadj pin is shorted to GND, and we are currently looking…
Part Number: LMZ31710 Tool/software: Hi I need to know the value of inductor embedded inside LMZ31710, its current rating and what is the percentage of ripple current considered. Thank You, Raju
Part Number: LMZ31710 Hi,
The datasheet mentions a minimum output capacitance of 500 uF for 0.6 - 0.8 V VOUT range. Does this mean only the local output capacitors or including the load side decaps?
Thanks,
Bharathkumar
Part Number: LMZ31710 Other Parts Discussed in Thread: TPS84259 Tool/software: Hi,
I have used LMZ31710 DC DC Convertor in one of my designs for 12V to 4V conversion. In this regard, kindly suggest EMI filters (IC), that can be used at the output of…
Part Number: LMZ31710 Tool/software: Hello, I have a project input 12V, output 1.8V, load 1A to 10A process, voltage drop after starting. I would like to inquire about the circumstances under which this problem may be caused.
Part Number: LMZ31710 Tool/software: Hi TIer
I see there some requirement with Cin in datasheet 7.3.4.2.
I saw this non-ceramic capacitance was suggested to be added to improve the load adjustment rate, but my customer is using sensitive power…
Part Number: LMZ31710 Other Parts Discussed in Thread: TPS54020 Tool/software: Hi,
I have used couple of LMZ31710 in my design. Power Good of first device is connected to INH pin of 2 nd device. I have noticed one strange behaviour.
As per the datasheet…
Part Number: LMZ31710 Tool/software: Hi
I have a input coming to LMZ31710. I want to use UVLO such that when the input is stable 10V then only my LMZ31710 should be active. If not it should disable the regulator can I do that. Regards, Raju