Hi Bob,
I frequently use the copy/paste method for projects in CCS5.3.0 without any problems. Here is how I do it:
1. Right click at the Project and select "copy"
2. Right click in the project explorer and select "paste"
3. in the pop-up "Copy…
Hi Keerthy,
After applying patch full log
I/TC: Dynamic shared memory is disabled [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 4.19.38-g4dae378bbe (root@techm-XPS-8500) (gcc version 8.3.0 (GNU Toolchain…
The SDK that you are using => 04.02.00.09
the console boot log => attachment
The file name of the function you are referencing? => /opt/ti-processor-sdk-linux-am335x-evm-04.02.00.09/board-support/linux-4.9.59+gitAUTOINC+a75d8e9305-ga75d8e9305/drivers…
Hi Imelda,
Thanks for reaching out with this question. What we would recommend here is that customers look at the impedance of their PoC network across the operating frequency range of the device. This would cover the forward channel and the back channel…
Other Parts Discussed in Thread: MSP430F5510 Hello, I am writing the USB enumeration firmware for a TI MSP430F5510 to be identified as a CDC type for a host running a Windows operating system (virtual COM port). In the past I have successfully written…
Hi Kazuya,
It can be opened with version 12. Usually you cannot open a MathCAD file if you are trying to open it with an older version of MathCAD not a newer one.
Maybe MathCAD trial version can not open this MathCAD file. I suggest customer to use…
Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 , PMP , WL1271 i arm use the OMAPL138 of custom board. The wifi module is wl1270 .
I use the drivers according to http://processors.wiki.ti.com/index.php/OMAP_Wireless_Connectivity_OpenSource_WLAN_release_R4SP2_Engineering_Drop#Kernel_build_…
Part Number: TCA8418 Tool/software: Hello!
I have encountered a bug where, in between a correct key press and key release event, I would get a false key press and key release. This does not always happen, and when it does, it is very brief. Not only…
Dear Don Dapkus,
we are through with audio codec registration. McBSP2 setting is fine we are able to probe BCLK and WCLK.
but in "alsamixer" setting there is no chip name is listed but for aplay -l its showing chip name. we have done ALSA library…
Thanks for the directions..
I keep modifying my code and now with a little code adding I get the same error back. I looked into my memory configuration with George's suggestion and I realized that I have so much memory unused (below). I tried to combine…