Part Number: BQ21040 Other Parts Discussed in Thread: LP38692-ADJ , Hi,
I have ordered bq21040 from element14 and designed the circuit on the breadboard as per the schematic in the datasheet for Ichg = 540mA. I am using an adjustable regulator lp38692-adj…
Part Number: LP38692 Hi,
I have used LP38692SD-ADJ/NOPB in one of my board which can take Vin up to 10V and i am generating 3.3V, for some reasons after testing my boards we need to generate 3.3V from 12V which will call for board respin.
I am thinking…
Part Number: LP38692 Other Parts Discussed in Thread: TPS7A45 Hi,
I have used LP38692SD-ADJ/NOPB in one of my board but now i want to use a LDO which can source output current greater than 1.2 Amp and voltage 5V with input 6V and should be footprint compatible…
Mike,
I have supported the LP3869x family since the release, and this is the first time I have heard of this particular behaviour.
I can take an LP38693-5.0 eval board the the bench this afternoon to see if I can duplicate. I also have LP38692-ADJ set…