Part Number: TLV755P Hello,
I am considering using the TLV75533PDRVR and LP5912-3.3DRVR in the same layout. This is in response to the recent difficulty in obtaining parts. The packages are the same, and the pinouts are generally compatible. Can both devices…
Part Number: LP5912-Q1 Hi,
Good Day.
In the datasheet for this part, it states on Page 5 that the dropout voltage is not a valid condition for output voltages below 1.6V. Since this part is a fixed output LDO of 1.1V, what does this note mean?
Let me…
Part Number: LP5912 Other Parts Discussed in Thread: TPS7A94 , TPS7A90 Hi,
I am currently in the process of sourcing an LDO chip with the view to taking input power from a 3.7V(nominal) LiPo battery.
I am after a low noise (powering op-amps etc), 3.3V…
Part Number: LP5912 Other Parts Discussed in Thread: TPS745 Hi team,
2uF is used for the output capacitor of LP5912. However, 10 ADCs are connected to the load and 10uF is used for the bypass capacitor of each ADC. The total amount of capacitors on the…
Part Number: LP5912-Q1 Other Parts Discussed in Thread: LP5912 Hi,
Is this part susceptible to latchup?
Do you have or aware of radiation test data (SEE, TID)
Is the part bipolar technology
Part Number: LP5912 Other Parts Discussed in Thread: TLV751 , TPS7A87 Hi
We are looking to upgrade the max current of the LDO we are using (the LP5907QMFX-3.3Q1 with max 250 mA) with a new one with more current (for example the LP5912).
Is there a similar…
Part Number: LP5912 Hi,
I am looking for a LDO for my customer to reduce the noise. Below is the requirements:
Vin,min < 2V
Vin,max > 5V
Vout,max >=4.4V
Vout,min < 1.2V
Output discharge
Iout(max) = 500mA
PSRR >= 70dB @ 1kHz
IQ(max): <…
Part Number: TLV755P Other Parts Discussed in Thread: LP5912 , TLV755 Can the LP5912-3.3DRVR be placed on the TLV75533PDRV footprint - it looks like the GND pin 3 is different but the thermal pads would be grounded.
Noted that the LP5912 output cap is…