Part Number: LP5912 Other Parts Discussed in Thread: TPS735 , TPS7A26 , TLV755P , TPS745-Q1 , Hi,
There is a long lead-time on the LP5912-3.3 WSON device, is there another LDO which could work as a pin-compatible drop-in? I have tried but to no luck managed…
Part Number: LP5912 We found max output capacitance value is 10uF in datasheet P7.
If customer use following part and over 10uF as output capacitor, Please tell me what kind of phenomenon at VOUT is seen ?
LP5912-3.0DRVT,VIn:3.3V
Regards,
Hi Kura,
There must be something in the system that is causing the LDO's to not turn on. Can you comment on Kyle's question above regarding the negative 400mV voltage? If the device is experiencing a voltage below abs max, it may be damaged.
…
Part Number: LP5912-Q1 When using this chip LP5912-Q1 to reduce voltage from 3.3V to 1.8V and 1.5V, what should be set respectively?Is there a reference circuit?
Part Number: LP5912 Tool/software: WEBENCH® Design Tools Hi experts,
i am using LP5912-1.2DRVT and LP5912-1.8DRVT fixed output DC-DC converters. in schematic i am using 5V input voltage and 1.2V, 1.8V output voltage but When i am simulating it in webench…
Part Number: LP5912 Other Parts Discussed in Thread: LP5907 We use linear voltage regulator IC, LP5912-1.2DRVR & LP5912-1.1DRVR, in our product.
By our customer request, we need to measure the Transient Response.
Vin is 1.8 V, ΔV is much higher than…
Part Number: LP5912 Hi team,
My customer would like to know if it is safe to operate the LP5912 up to 550mA continuously, assuming they could take care of the thermal dissipation.
the application will be regulating Vin of 5.2 ~ 5.4V to output of 5V, so…
Part Number: LP5912
Hi, I have a little question. I am using LP5912-1.5DRVT 1.5V version.
Can I use multiple LP5912-1.5DRVT as parallel ? Lets say three of them.
They will use same input 5V and their output will be shorted.
Thank you,
Best Regards.