Part Number: LP5912-Q1 Other Parts Discussed in Thread: TPS7A88-Q1 , Hi,
My customer is looking for a TI device with below requirements. Can you please suggest something?
This is automotive customer so please share Q1 device.
Noise requirement: 2nV/sqrt…
Part Number: LP5912-Q1 Hi There,
Please could someone check the schematic attached and provide any feedback on changes required? This is for an automotive cluster design taking the 3V3 rail and dropping the voltage to 3V. All resistors are rated @ 5%…
Part Number: LP5912-Q1 LP5912Q1.5DRVRQ1 the Datasheet show that when Vin-Vout = 0.5V is the best status。But we want 1.8V in ,1.5V out, The performance is OK?The I-out = 350mA.
Part Number: LP5912 I'm considering using the LP5912 3.3V part for a new application. I will need to connect "EN" directly to "IN" and am wondering if the Output Discharge FET will still be active when powered down. I don't have the eval board yet…
Part Number: LP5912-Q1 Other Parts Discussed in Thread: TPS3700-Q1 , TPS3702-Q1 Hi There,
I am using the LP5912-Q1 as a 1V2 linear supply off of a 1V8 PMIC SMPS output.
Looking at the PG function of the regulator I think I understand this as : the PG is…
Part Number: LP5912-Q1 Hi team,
I would like to run a thermal simulation of LP5912-Q1.
Is the model for below simulation tool available for this device?
1) FloTHERM(.pdml)
2) ANSYS Icepak(.tzr)
・LP5912Q3.3DRVRQ1
・LP5912Q1.8DRVRQ1
regards,
Part Number: LP5912 The data sheet indicates ABS MAX for PG and EN pins as 7V, irrespective of the VIN voltage. Please verify that the PG and EN voltages can be above VIN as long as they are below 7V.
Thanks,
Mark