Part Number: LP87524-Q1 Have been trying to create a DTS file for a LP87524 on i2c bus 1 address 0x60, I have what appears to be a overlay that compiles and runs however my initial values are not being set on load.
I've used https://elixir.bootlin.com…
Part Number: LP87524-Q1 Hello,
I am now trying to use a LP87524 q1 DC DC converter to convert a voltage from 5V into 3.3V, 2.7V, 1.8V and 1.2V. And because 4 different output voltages are needed, I will choose the configuration of four 1-phase outputs…
Part Number: LP87524-Q1 Hi team,
Can I measure phase margin and draw a bode plot of LP8752x-Q1 by inserting series resistor in between OUT and FB_Bx pin?
regards,
Part Number: LP87524-Q1 Hi Expert,
I don't really understand what's the current limit for each channel. I don't see clear description about this. what does it mean by "The maximum output current from....phase configuration"? The total current is less…
Part Number: LP87524-Q1 Can LP87524-Q1 not connect to I2C?
If it does not connect, can Control Registers be shipped in a hard-coded way when it leaves the factory?
Part Number: LP87524-Q1 Hi team,
if configure the LP875230-Q1 to 2+1+1 mode, what's the current limit in each phase?
the total current limit of LP875230-Q1 is 10A, right? how about the each phase? How to distribute the current of each phase?
thank…
Part Number: LP87524-Q1 Hi team
Here we have encountered a issue that when LP87524 outputs abnormally. When the EN is high (green waveform), the LP87524Q1 output is 1.8V but when EN from high goes low, the LP87524Q1 output is abnormal and the voltage value…
Part Number: LP87524-Q1 Hi team,
My customer is planning to design LP87524-Q1 but they would like to know the difference between all LP8752x series devices.
And could you also advise the LP87524's default value setting?
And does customer need to do…
Part Number: LP87524-Q1 Hi Team,
I noticed that the LP87524 register map doesn't include anything for slew rate control, which appears to be default set by the OTP to be 3.8mV/us. Is this an OTP-only register, or is there another address that we can write…