Part Number: LP87561-Q1 Other Parts Discussed in Thread: LP8764-Q1 , LP8758-B0 , LP8758 Hi sir,
The LP87561 is out of stock, can you recommend the 16A PMIC that it has differential sense from C load to use?
Part Number: LP87561-Q1 hi team,
could you kindly help understanding the differences between these two part#?
LP875610RNFTQ1 vs LP87561IRNFTQ1
Could you please help pointing out where to find in the datasheet? Thanks! Best Regards, Brian
Part Number: LP87561-Q1 Hi,
Do we have IBIS models for this family of devices? I've found other simulation models on the product page but was curious about this one as well.
Thank you.
Part Number: LP87561-Q1 Hi,
I had a doubt regarding the Current Limit Functionality for this part. Let's say it is used in a 4 phase application for a VOUT of 1V and normal load current of 2A. Assume the "ILIM_FWD" current setting is set to 4A for all…
Part Number: LP87561-Q1 Hello TI friend.
I downloaded the simulation model " lp875x_ac_transient_simulation.sxsch". And run in the SIMPLIS without change any parameters.
But the bode curves is not same with the technical article from "…
Part Number: LP87561-Q1
Hi,
Will the over voltage monitoring functionality using POWER GOOD work even if the sense line (connected to FB_Bx) is floated?
Say I've enabled the over voltage monitoring functionality for PGOOD. If by mistake, in the 4-phase…
Part Number: LP87561-Q1 Hello Guys,
I might have missed it on the datasheet but what is the difference between LP87561 0 RNFRQ1 and LP87561 I RNFRQ1 ?
Thanks in advance!
Art
Part Number: LP87561-Q1 Hi Expert
I am looking for 1mV output ripple solution, for 3.3V to 0.94V / 10A.
LP875761 looks good, but its Vout is fixed at 1V.
LP87561 seems to be the closest one, but still it needs more optimization on L/C to try.
Do you have…
Part Number: LP87561-Q1 Hi,
In the datasheet, the Output filtering capacitance per phase, ie Cout_Local is mentioned as 22uF typical. In the application report "Stability Considerations for LP8756x-Q1 and LP8752x-Q1" also, looks like Cout_Local used per…
Anoop,
This question has been assigned to the experts on the LP87561-Q1 device but they are based in Europe and I do not expect you will receive a response until Monday.