Part Number: LP87561-Q1 Hello
When I using the lp87561-q1, I found that the power output was only 0.9v, but I want it to be 1.0v.
We need to write registers to output 1.0v.
1. May I ask whether TI supports the fixed output of the version 1.0v? Which…
Part Number: LP87561-Q1 Hello Team,
I was wondering what the Maximum Load Current givein the Table 1 of the Technical Reference Manual means?
http://www.ti.com/lit/ug/snvu513a/snvu513a.pdf
This is a 16A part but in the table 14A is give as the maximum…
Part Number: LP87561-Q1 Other Parts Discussed in Thread: LP87565-Q1 Hi,
Here are some questions:
1. What's the MP schedule of LP87561-Q1/LP87565-Q1
2. LP8756x have different version, but there is only LP87561 have sample can be applied. Will other…
Part Number: LP87561-Q1 Hi Team,
May i have your help to confirm the LP87561-Q1 has only one I2C address 0x60? is there more options for the I2C address?
Regards,
Henry
Hi,
LP87571-Q1 is special OTP version created to meet certain processor power supply requirements and it is more useful if you use this device as it is configured in its default OTP. I recommend LP87561-Q1 for your application and adjust the output voltage…
Part Number: TPS650864 Other Parts Discussed in Thread: TPS6593-Q1 , TPS65023-Q1 , TPS6594-Q1 , LP87564-Q1 , LP87561-Q1 , LP87565-Q1 , LP87562-Q1 , LP87563-Q1 , LP8764-Q1 Team,
Is there any alternative part recommendation for TPS650864X which is AEC qualified…
Hello,
TPS650864 has a UVLO detection circuit on VSYS pin (low current) which requires > 5.6 V, so a small boost like LM2667 is required for it to operate with only a low voltage high current supply like 5V instead of 12V.
A few multiphase devices…