Part Number: LP8758-E0 Hello - I'm using the LP8758-E0 in a design that could be operating in high heat conditions so I would prefer to use X7R capacitors for the output and input. However the smallest 22 uF X7R caps are in a 1206 package, and the…
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758 , Hi Team,
My customer is looking at using this LP8758 device, but one of their main concerns is it's thermal behavior. Do you think a heat sink will be required when using this device at its…
Part Number: LP8758-E0 Hello. I have a question.
The LP8758-E0 looks good for my FPGA power supply.
I need a total of four power rails : 1.2V, 1.8V, 2.5V, 3.3V.
But the LP8758-E0 is set to 1V, 1.2V, 1.8V, 2.5V.
The LP8758-E0 uses OTP, so the default power…
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758 Hi,
Can the LP8758-E0 start up VOUT0~3 without I2C control as below?
Best Regards,
Kuramochi
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758 Ordering the LP8758-E0 with pre-programmed voltage on all 4 outputs. I want to know the lead time for these device with pre-programmed voltages. My understanding is that there is a one time…
Part Number: LP8758-E0 Hi,
My customer is using LP8758-E0 to supply PLL in 400Gbps optical module. They need to minimize the switching noise of output voltage to achieve better eye diagram. I've suggested adding a snubber at switching node and optimizing…
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758 Test case description
LP8758-E0 ("LP") is used to supply 4 voltage rails.
Rail 0: 1.0V Rail1 : 1.8V Rail2 : 1.2V Rail3 : 1.8V
Vin=5V EN2 which is programmed to be enable/disable…
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758-E3 Hello
our customer use LP8758-E3 , Vin=3.3V; Vout0 =0.9V, when the output current changes from 1.5A to 1.8A suddenly, the Vout0 changes from 0.9V to 0.83V.
is there any suggestions on this…