Part Number: LP8764-Q1 Hi TI team,
I would like to check with you for the L inductance value buck 3 of LP8764-Q1.
You guys have recommended me typical value of 470pF, but could it be lower for 330nH?
As schematic figure below, I am going to change…
Part Number: LP8764-Q1 Other Parts Discussed in Thread: TPS6594-Q1 We have an LP876441B1RQKRQ1 PMIC on our new design PCB which is not responding with data when we read the I2C.
We measured VCC=5.0V, VIO=3.3V, VOUT_LDO=1.8V, initially there was some residual…
Part Number: LP8764-Q1 Other Parts Discussed in Thread: LP87563-Q1 Dear Team,
I have plan to use LP8764-Q1 part in my new design.I got some doubts on the current monitoring feature of LP8764-Q1.
In device datasheet section 8.7 output voltage monitor and…
Part Number: LP8764-Q1 Hi
We use the LP8764-Q1 on our automotive project. the condition is: 1. the RECOV_CNT_REG_2 (RECOV_CNT_THR) value is set to 0. 2. we turn the GENERAL_REG_1(REG_CRC_EN) to the "register CRC enable".
We use the Linux command…
Part Number: LP8764-Q1
Hi TI team,
I am facing UV problem for LP8764-Q1 on system reliability qualification. The fault report as following:
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5a r1
0x91
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5b r1
0x0…
Part Number: LP8764-Q1 I am facing UV problem for LP8764-Q1 on system reliability qualification. The fault report as following:
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5a r1
0x91
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5b r1
0x02
mfg-s32g> i2ctransfer…
Part Number: LP8764-Q1 My laptop do have Ticloudagent already installed as well as the TICloudagent bridge is already active in the browser extension.
Still when I try to use the Scalable PMIC GUI via the web link
https://dev.ti.com/gallery/view/PMIC…
Part Number: LP8764-Q1 Dear,
We would like to use the LP8764-Q1 PMIC in one of our own designs. However, this would require programming a specific configuration to the device. From the LP8764x-Q1EVM, it is clear that this is possible using the scalable…
Part Number: LP8764-Q1 We have an LP8764 part on our board, and we have programmed it with new config files several times with no issues. However, the last time we tried to re-program it, it always gives us error that "EEPROM Unlock Failed". My question…
Part Number: LP8764-Q1 Other Parts Discussed in Thread: MSPM0L1306 I am trying to implement a very simple state machine.
When enable rises it should execute a power up sequence.
When enable falls or the input power falls it should execute a power down…