Part Number: LP8866-Q1 Configure the LP8866 into Direct PWM mode. It could be capable to change the PWM directly from 10% to 80% (instead of slowly adjust), right?
Thanks!
Part Number: LP8866S-Q1
Hi Team,
just want to check the current consumption when EN is pulled low.
datasheet provide Iq in shutdown mode which is 5uA.
There are still several point except Iq, is there leakage current data into below pins @ Vin=12V, EN…
Part Number: LP8866S-Q1 We are using one the TI LED Driver IC, with part number-LP8866SQDCPRQ1 (TSSOP package), in one of our designs.
We are facing an issue on the same and below is the issue description.
Initially, the board boots up and the TFT Screen…
Part Number: LP8866-Q1 Other Parts Discussed in Thread: LP8866EVM Hi Team,
In datasheet, I saw below words.
Below is our setup, but the LOD wasn't detected again.
1. LP8866 in normal work
2. Remove LED board
3. LP8866 LED status showed the LED open…
Part Number: LP8866S-Q1
Hi,,
I would like to design Sepic Converter for LED DRIVER LP8866S ( We use ic LP8866SQDCPRQ1 ). Refer to AN-1484 Designing A sepic Converter- SNVA168E and LP8866S-Q1 LED DRIVER from Texas Instrument (TI)
And want to know the right…
Part Number: LP8866-Q1 Other Parts Discussed in Thread: USB2ANY Using the LP8866 EVK. I am just firing it up and got the USB2ANY updated with the latest code. When I try to fire it up I get an error message:
"Connected to USB2ANY Controller, but failed…
Part Number: LP8866-Q1 Is there an empirical value for the two packages of LP8866, how much power can it support? The PCB is a 6-layer board, and the load is 13W, 400mA, 31.9V.
How to accurately calculate whether QFN can meet the requirements of thermal…
Part Number: LP8866-Q1 Hello,
This part has been designed into an automotive ECU. My task is to take advange of the LED driver's feature by switching from PWM control to I2C control.
Reading the datasheet, I decided to control the PWM with BRT_CONTROL…